Part Number: AFE2256
Hi Expert,
One of my customer is evaluating AFE2256, here is some questions from them, could you help on this?
1. Vbias: Is it fixed or variable? if fixed, what is the voltage?
2. VCOM1-4: Is that ok to connect VCOM1-4 to ground? If not, how do they deal with them?
3. Do you have Timer Profile initialization example?
4. Do you have SPI initialization example?
5. Do you have using LVDS to read ADC data example?
Regards,
Yangbo