Part Number: ADS124S08
Hi Team,
The customer is experiencing below issue and needs your help.
- If the ADC Data rate is set to 10sps, is the maximum SPI output data rate 10sps?
- If the ADC Data rate is set to 10sps, choose 6-channel data acquisition, how to ensure that the 6-channel alternating data acquisition rate (using Low-Latency Filter filtering) and ADC Data rate are synchronized?eg: The output channel data is output in the order of ch1, ch2, ch3, ch4, ch5, ch6, ch1, ch2, ch3, ch4, and ensure that the output is synchronized with the ADC Data rate.
- If the ADC Data rate is set to 10sps, select 6 channels of data for alternate acquisition (using Low-Latency Filter), can power frequency noise be suppressed for each channel?
Thanks,
Annie