Part Number: ADS8568
Other Parts Discussed in Thread: ADS8688A, OPA209
Hey everyone!
I've looked at the ads8568 briefly in the past but now need to implement it in a design.
Concerning the output data format in serial mode. If I have this correctly the format looks like it uses spi or qspi depending on how many output pins are chosen. I'm not sure whether I'm analyzing the serial timing diagrams incorrectly and whether another peripheral would better suit it?
Concerning the input signal, It seems that the input is a single ended true bipolar and thus the full range runs over a the span from a negative to positive reference value. My input signal however is Unipolar and DC. It will vary between 0 to 5V, I thus want to know whether there is a signal conditioning I can apply to get my input signal to span the whole bipolar range. So a conversion where the the input signal is conditioned from say 0 -> 5V to -5V -> 5V.
some key points of the signal will then be
original -> new
0V will become -5
2.5V will become 0V
5V will be 5V
Thanks in advance for any help!