Other Parts Discussed in Thread: THS4521
I had already posted about this issue I had with 1 out of 10 new revision (REV D) boards here https://e2e.ti.com/support/data-converters/f/73/t/896978
I originally thought I just got a bad chip on the 1 board, and sent it back to the assembly house to have it replaced. Got the board back and it is working ok so I had closed the issue.
Now on an additional board, which had been working fine, the same issue has occurred where all the DOUT lines are low. Nothing changed in the design or layout with the ADS1278 from REV C to REV D, and there are REV C boards that have been running for over a year without any issues.
I do connect AGND and DGND with a ferrite bead close to the ADC. When I measure the potential between AGND and DGND it is only ~20-25mV which is well within the specs, so I wouldn't think that is the problem, and the grounds are connected this way on the REV C boards which have never shown this issue.
Any additional help would be appreciated.
Thanks,
Eric