Part Number: ADS1255
Hello,
I have checked many threads related to read data continuous mode and sometimes there is mentioned: "Also, after RESET, the device will default to RDATAC mode", see https://e2e.ti.com/support/data-converters/f/73/p/889689/3292609.
Can someone point me out to the ADS1255 datasheet where there is specified that the data continuous mode is the default one? I do reset via RESET/ pin and this information would be very important. What I have observed so far, the WREG command + register data is ignored right after reset and there must be ~600 us delay (it does not depend if DRDY/ is high/low) between RESET/ goes high and first WREG command.
BR
Martin