This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS125H02: samping-rate and data rate

Part Number: ADS125H02


Hi Sir 

   How can I calculate the real ADS125H02 samping-rate and data rate?

   I used 7.3728MHz external clock, configered the register as follower.

   writeSingleRegister(REG_ADDR_MODE1,MODE1_CHOP_ON | MODE1_CONVRT_CONTINUOUS | MODE1_DELAY_50_uS);

   writeSingleRegister(REG_ADDR_MODE0,MODE0_DR_25600_SPS);

   The nDRDY pin signal is about 4kHz.

Best Regard

Kai Yu

  • Hi Kai,

    You can actually use the ADS125H02 online calculator to determine the conversion time for your settings. The link is here.

    I have copied a screenshot from this tool as shown below. With chop mode = on, delay = 50us, and 25.6kSPS data rate, the first conversion latency is 0.52 ms, while second and subsequent conversions on the same channel take 0.25 ms. This does not account for any error in your clock signal, and is a good estimate.

    -Bryan

  • Hi Bryan,

        thank you, it makes sense. The calculation is very accurate.

    Regards,

    KaiYu