Part Number: ADC12DJ5200RFEVM
We used to use ADC3200EVM and we are moving onto ADC12DJ5200RFEVM. HSDC Pro is the same with the patch. We did follow the instruction and were able to make the ADC12DJ5200RFEVM now and them up to 4GHz or so and wer were experimenting with it to push the speed to 10.4G. But along the way the ADC12DJ5200RFEVM stopped being recognized by WIN10. We uninstalled and re-installed both programs and drivers multiple times to no avail. Power to the board is fine and we tried multiple USB cables. It has become un-expected road block in integrating this board in our testing prep...
Anything we could be missing?
Regards,
Mesfin