Other Parts Discussed in Thread: ADS124S08
The EVM has been working satisfactorily under Windows 10 Home (10.0.18362 build 18362), but it is grounded through the USB port, which is causing excessive noise. I bought a USB isolator, SEEED studio 114991949 (which actually came in a box marked 52Pi) This works correctly on a Windows XP machine for a flash memory stick, and also on a Picoscope 3206 USB oscilloscope. It also works correctly for the same flash memory stick on the Windows 10 machine.
When the EVM is plugged in via the isolator you get the Windows connecting sounds, but no connection to the TI Delta-Sigma ADC evaluation software. The green LEDs on the eval board light up. The TivaWare Bulk devices report in the Device Manager is:
“This device cannot start. (Code 10)
Insufficient system resources exist to complete the API.”
The driver is Texas Instruments 2.1.4.0 from 18/10/2016.
When the EVM is working correctly, the driver says it is working properly, but I wouldn’t say it was “happy”.
------------------------------------
Information box:
Device USB\VID_1CBE&PID_0003\12345678 was not migrated due to partial or ambiguous match.
Last Device Instance Id: USB\VID_0D8C&PID_0005\201306
Class Guid: {36fc9e60-c465-11cf-8056-444553540000}
Location Path: PCIROOT(0)#PCI(1001)#USBROOT(0)#USB(3)
Migration Rank: 0xF000FFFFFFFF0023
Present: false
Status: 0xC0000719
----------------------------------------------------------------------------------------------------------------
I have deleted and reinstalled the driver, and re-installed the delta-sigma ADC software.
I found https://www.repairwin.com/fix-usb-device-cannot-start-code-10-error/
and disabled power saving in the USB driver (method 1). There were no upper or lower filters (Method 2). My machine has an AMD A10-7800 Radeon R7 processor so intel drivers (Method 4) seem inappropriate.
Is there a better driver available? Or any other suggestions?