Part Number: ADS1256
Other Parts Discussed in Thread: OPA350, REF6025, ADS1255
Hi!
I look all answers related to ADS1256 oise but still I do not find a solution for my problem. So, here I am asking on my way: is this level of noise acceptable for my configuration or not.
I think it is still too big....
1.) For the start I bought this ADS 1256 board: www.aliexpress.com/item/2046677415.html
I am using this module in combination with Arduino Mega2560.
After almost one week I managed to operate with this moduel and I am getting approximately correct results.
2.) After that I made my own dev board with ADS1256, to be sure that I know hot to manage with this chip. After few repairings, my module works,too.
But now, I am testing the performance of my board and the module I bought from internet anbd I found out, that according to my opinion, the nosie level is too big,
at the bought module and on my own.... The results are very similar:
Register settings on both modules are the same:
PGA=1, buffer =Off, sampling speed I changed: 500SPS, 1000SPS and 30000SPS. I am using only signal from 0 to 5V, single ended measurement. The 5V signal I generate with precise 5V calibrator, battery power supplied. AINCOM I have connected to the AGND. Analog and digital ground are separated, connected together only in one small point under the ADS1256 chip...
Here are the results @5V DC input signal. I memorized the minimum and the maximum value:
5V @500spsp:
My module: MIn=7827738, MAX=7831099, difference=3361
Bought module: MIn=7819528, MAX=7822641, difference=3113
5V @1000spsp:
My module: MIn=7826321, MAX=7830670, difference=4349
Bought module: MIn=7816679, MAX=7820689, difference=4010
5V@30000sps
My module: MIn=8343959, MAX=8352881, difference=8922
Bought module: MIn=8334841, MAX=8344354, difference=9513
So the results are logical, less sps I have , the difference etween the min and max value at the same voltage is smaller. But I think this difference is still too big....
For example the difference @500sps is app 3000, comparing to full 23 bit value=8388607 this represents 0.035%.
Is this according to expected? I expect less than 0.01% oe am I wrong? Did I miss something?
Thank you for your help and best regards!