Part Number: ADS1299
Hello. Sorry, I didn't find full information about acceptable noise value when input shorted in ADS1299.
(in this link, a similar problem like and my situation, but Mr. Brian said - OK e2e.ti.com/.../547117
If I shorted the channel input (by register CH1SET - 0x01) I receive the next result for the channel -
867
866
865
862
if convert to volts = 461 mkV it is too much. (error = 862*2*4.5/16777216)
if I shorted the input channel external by cable I receive similar value, with PGA gain = 24 my result will be 20 mkV. But it is too big.
Which value I need to receive during input shorted for the correct measurement EEG signal?