Hi TI Engineer:
Question 1: Regarding ADC32RF80EVM board, the recommended data acquisition card in the description on TI official website is TSW14J56EVM. Can I use TSW14J57EVM data acquisition card for sampling?Meanwhile, regarding ADC12DJ3200EVM board, the recommended data acquisition card in the description on TI official website is TSW14J57EVM. Can I use TSW14J56EVM data acquisition card for sampling?Do you have any problems with this match?
Question 2: Due to special needs, now it is necessary to stitch two ADC32RF80EVM boards with 3G sampling rate to achieve the effect of 6G sampling rate (two chips are sampled alternately). Is this possible if I use LMK04828BEVM boards for clock control of two boards?The main concern is the control accuracy and response time of LMK04828BEVM.How much error can this scheme achieve?