Part Number: ADC32RF44
Hey team,
Quick question regarding the ADC32RF44, can a SPI reset be used instead of the hardware reset on startup?
Thanks,
AH
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi AH,
Hardware reset is required as shown in the initialization sequence in datasheet.
Two corrections:
Step 2 should be "Provide input clock and SYSREF signal"
Step 3 should be "Pulse hardware reset (low-to-high-to-low) on pin 48" (not pins 33 and 34)
Hardware reset timing is specified in the datasheet as below:
Regards,
Vijay