Other Parts Discussed in Thread: TPS63802, PCA9306
Hi,
I am planing on using the ADS1119 in a system to measure temperature with NTC thermistors but I have some doubts on which power supply architecture is best. The board will be powered by a single Lithium Ion cell. Under normal circumstance ambient temperature will be around 0ºC. From the data sheet of a Panasonic NCR18650 (https://datasheet.octopart.com/NCR18650B-Panasonic-datasheet-34154111.pdf), at 3.3V (needed for the uP) there will be still about half of the energy left in the battery. I guess using a buck-boost converter like the TPS63802 solves this issue but, on the other hand, noise might be become problem so I probably need a low noise LDO for the ADC and the NTC's, perhaps a LP5907MFX-3.0. Now, given that the uP will be powered directly from the DC/DC converter and the analog subsystem (i.e. ADC and thermistors) from the LDO should I:
a) supply both the ADC's VDD and AVDD plus NTC's from the LDO or
b) supply ADC's VDD from the DC/DC converter and AVDD plus NTC's from the LDO
To make things more complicated, the uP will be in deep sleep mode mode most of the time and wake up to take a measurement every 5 to 30 minutes so I can't keep the NTC's on during sleep. Option a) would allow me to power down the ADC and the NTC's by simply shutting down the LDO with the EN pin but possibly creating problems with other devices on the I2C bus and the ADS1119 itself. Option b) on the other hand would keep the digital side of the ADC powered at all times while shutting down only the analog side but I am not sure if this an option at all.
I would greatly appreciate some advise. Perhaps I am over engineering this and there is a simpler solution.
Best regards and many thanks in advance,
Christof