Part Number: ADS1299
Hello TI forum,
I am trying to use the ADS1299 to acquire 8 channels of EEG data at a rate of 8kHz. I will also need to configure the ADS1299 for proper operation, including setting of the programmable gains, the reference and bias electrodes, leads-off detection, etc.
Has anyone written or know where I can get an example Linux device driver for the ADS1299?
I realize that I will have to adapt it to my own hardware, but the basics of writing to and reading from the various internal registers should be the same. Of course, the SPI interface will need to be customized based on our processor hardware.
Any assistance that you can provide so that I don't have to reinvent the wheel would be greatly appreciated.
Please feel free to ask other questions for clarification if needed, and thanks for your time and help!
Scott