Part Number: ADC08D1520QML-SP
Customer is using the ADC08D1520-SP and has a scenario where one of the inputs on one channel, (VINI+ or VINI- for example) could very infrequently see an overvoltage transient condition of 2.8V for < 1msec. This exceeds the max voltage rating for the pin of 2.5V. There is also an input current max rating of +/- 25mA. Note (3) under the table indicates the voltage can exceed VA if the current is limited under 25 mA.
Can they exceed the absolute max rating of 2.5V with the 2.8V transient for short durations on the input without permanent damage as long as the current is limited under the 25mA absolute max rating?