Other Parts Discussed in Thread: ADS1263,
Hi guys,
my customer have been using the AD7730.
Thanks to your recommendation we suggested the ADS1263 but the customer preferred to test the ADS1261EVM. He has some questions:
First problem: the offset register is unique, for internal and external calibration. Perform an initial calibration without laod. During normal operations it is not possible to continuously calibrate the offset to compensate for drift,carrying out an "internal calibration", which would override our offset, since the initial offset register contains our "tare".It therefore becomes necessary to store the offset in the external control system and continuously calculate the offset.
Second problem, and more serious: full scale calibration is not possible.It is not possible to calibrate the full scale with an "internal calibration" method because the converter does not have this function,it is not possible to calibrate the full scale with a "system calibration" method because our signal is too small.
With the GANCAL calibration command, the FSCAL calibration register takes the value 1FFFFF, therefore out of scale (<106%)
The converter works quite well, but these calibration errors make it problematic if not impossible to use.
Could you help us?
Thank you
Riccardo