4. Add a new one.
In the amc1304 datasheet 7.1 Absolute Maximum Ratings
The Analog input voltage at AINP, AINN voltage is ( AGND – 6 to 3.7 ) V.
And in the 8.3.1 Analog Input
" There are two restrictions on the analog input signals (AINP and AINN). First, if the input voltage exceeds the
range AGND – 6 V to 3.7 V,…. "
My question is what’s the mean of the “3.7V” ?
Is Agnd +3.7v or GND+3.7v or LDOIN+3.7V ?