Hi Team,
One of my customer are searching for a part having the features that 16bit, 4 to 20mA anlaog input with Bus voltage of 24V support, SPI interface, single channel ADC. Our application is to interface with HS 420 vibration sensor and collect the digital data through SPI interface. Please support us to find the same part.
It is simple to select ADCs using Resolution(Bits), interface and number of input channels at TI's web page, but I do not know how to select using "4 to 20mA anlaog input with Bus voltage of 24V support". Could you give me some advice?
Beat Regards,
Tom Liu