Other Parts Discussed in Thread: ADS1178, , ADS1274, ADS1174
I have two daisy-chained ADCs on a board and cannot get the ADS1278 to give any good data or transfer any data from the ADS1178 behind it. When I reverse the order, the ADS1178 sends its data fine, and then the gibberish the the ADS1278 sends it. It is almost like the ADS1278 is in modulator mode. Setup below:
CLKDIV : 1
Mode[1:0] : 1,1 (Also tried 0,1)
Format[2:0] : 0,0,1
Test[1:0] : 0,0
CLK; 24 MHz
The ADS1178 setup is the same except for no Mode 1.
Power up sequence: 1.8, 3.3 and 5 V all start at the same time and have the same slope such that 1.8 and 3.3 reach the 1 volt threshold first, and the 5 volt reaches the 3 volt threshold about 6 ms later. I've tried holding off on the clock until after the startup, but no change in the data stream. I've tried this on 2 separate boards and both ADS1278 ADCs are exhibit the same behavior while the ADS1178s both work.
Any thoughts on what is going on here?
Thanks