Part Number: ADS1246
Hi,
Would you please help to review ADS1246 circuit?
thanks
regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Lee,
Apologies for the delay in response.
Looks like you've configured the device for continuous conversions, internal clock, and will collect data using the combined DOUT/DRDY pin.
I would recommend decreasing the size of the common-mode capacitors C49, C47, by 10x such that they are 10x smaller than the differential capacitor C57.
I would recommend reviewing section 9.3.2.2 PGA Common-Mode Voltage Calculation Example of the datasheet. I see that you are using bipolar 2.5V supplies. Tying the positive input to 2.5V via R2 will result in a common-mode voltage violation.