Other Parts Discussed in Thread: TLC2578, TLC3578
Dear Sir;
We have procured the samples of TLC2578 ADC. Currently we are facing the problems in SPI communication with the ADC.Could you please do the following needful,
1. C source file for SPI communication through MSP430 microcontroller with TLC2578.
2. When ADC's analog channel one is selected (which is connected to ground) for sample and conversion, The converted o/p was 0x9790 and 0x97A0.
When the same analog channel connected to +4.7volts , ADC converted value was 0x97C0.
When connected to -13volts , the converted o/p was 0x9740
Why the converted results are not proper and varying .
3 whether REFP should be connected to +10 volts ,when the ADC analog channel inputs are connected to +/-10 voltage inputs.
4. Whether AVdd and AGnd should be connected to +/-10 volts respectively , while analog channel inputs are working with
+/-10 volts.