This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8634: ADC Transitioning Data Without Clock Edge

Part Number: ADS8634

Hello,

I am using your ADC and have ran into an issue where the data out from it is incorrect periodically.

I am using channels 0-2 in auto mode with the 0-5V internal reference. The input signal is normally at 2.5V, with a few LSBs of fluctuation. 

Most of the time a valid ADC reading of 0x800 +/- a few LSBS, with the correct channel data preceding the ADC data is received.

However the ADC sometimes outputs incorrect data as shown below.

Yellow = CLK, Blue = MISO

(Yellow = CLK, Blue = MISO)

As can be seen there is no issue with the clock signal input to the device, so there is no reason for the output data to be toggled at the point that it is.

The high peaks and ringing on the signals have been confirmed to be a result of the probing setup (longer leads with crocodile clips) and are absent when probed with a proper ground spring setup.

A close up of the above signal.

Thank you for your help,

Jamie

  • Hi Jamie,

    Your waveform was not uploaded successfully. Please provide your timing plots including /CS,SCLK,DIN and DOUT for a good and bad data. The actual internal reference voltage on the ADS8634 ADC is 2.5V, I guess your are using 0-5V unipolar range with an 2.5V internal voltage reference. Also, please provide your schematic for a review.

    Thanks&Best regards,

    Dale

  • Communicating offline regarding Jamie's request, this thread will be closed.

    Best regards,

    Dale