Part Number: DAC5652AEVM
Other Parts Discussed in Thread: DAC5652A
Hello,
I'm trying to use the DAC5652A in my design. I have the EVM hooked up and am trying to generate voltages but am not seeing any output.
As per the EVM manual, I have applied 3.3V to both VDD and AVDD. I am supplying DA0-DA9 with increasing values from 0 to 1000 and supplying a clock on WRT1. I have J1 connected to an oscilloscope.
The timing and data on the bus and clock are shown below:
I am however, seeing nothing on J1. I have tried toggling SLEEP while the data is being clocked in. If it helps, the EVM board is drawing about 80mA when I power it on and clock in data.
What could I be missing?
Sincerely,
Aditya