Other Parts Discussed in Thread: ADC128S102QML-SP, MSP430F5529, ADC128S102
I plan to use the ADC128S102EVM without the launchpad. I have a few questions:
1. What is the thickness of the board? Since the board doesn't seem to have screw holes, I need to configure edge holders to hold the board.
2. Is there a launchpad breakout board that simply breaks out all of the I/O of the eval module and has mounting holes?
3. What are the part numbers for the J1, JA-JD connectors? The parts list in the users manual is outdated - the part numbers listed do not seem correct. I need to select cables to plug into thrm.
4. The parts list shows U2 (the ADC) as ADC124S.... This seems wrong. Just verifying.
5. My goal is to test the SPI interface used with the space grade adc128s102qml-sp. The ADC182S102QML-SP seems to be very similar to the ADC128S102CIMT, but differs in the SPI clk required and radiation hardening. Besides these differences, are the SPI commands/controls equivalent?
Thank you.