I am interested in using AMC6821-Q1 (Intelligent Temperature Monitor and PWM Fan Controller) in one of our board designs, where a four-wire blower fan is going to be used. The ~OVR, ~THERM, and ~FAN-FAULT signals will be used to shut down the board if an error condition is detected.
However, I would like to have the option of using either a two or three-wire blower as well, if for some reason the four-wire blower is not available. For operation with the two-wire blower, it appears that disabling ~FAN-FAULT in Configuration Register 1 would de-assert the signal, thus keeping an error from being thrown.
When using a three-wire blower the data sheet suggested that the power pin of the blower fan would need to be driven by the PWM output, which also enables the Tach of the Fan. I assume this configuration would provide both speed control and tach features.
However, the alternative three-wire fan that I am considering provides an open collector Tach output that can be pulled up by a resistor connected to a voltage. For this case, I would not need the speed control, as the fan would be running at full speed, but would still want to read the Tach. It seems that the PWM output could be disabled in the Configuration Registers after startup, allowing this configuration to work.
Unless I have missed something in the data sheet, it appears that the AMC6821 would support either two (power only), three (power and tach), or four-wire (power, tach, and speed control) blower fans by simply programming the Configuration Registers appropriately. I just would like some verification to make sure that I am correct with my assumptions.
Thanks.