I am esearcher from Ireland.
I would like to get support on products from TI.
I am looking for a 12-bit Current Steering DAC on an evaluation board with sampling frequency around 10-100 MHz
The DAC should be segmented 5:7 segmentation Nyquist rate
I would like to interface our digital solution implemented onto Xilinx FPGA board through FMC connector to MSB 5-bit DAC and have to take the measurement results for an overall 12-bit DAC
The DAC can take input as a 1.8V i.e. representing 1
We are looking for a single channel if there are two channels will be fine