Part Number: DAC8554
Other Parts Discussed in Thread: DAC8551
Hi everybody,
I have a board with DAC8554 and I am using SPI interface of Labview FPGA to communicate with the board. LDAC input of DAC8554 is grounded, ENABLE and SYNCH are connected to CS output of SPI interface. The first command I send after turning on the power works perfectly fine. I have tried many different commands and there is no problem in any. However, the second command doesn’t change anything. The only way to reprogram is to turn off and on again the power connection. There is no problem with the other chips I have on the board (i.e. DAC8551).
I would appreciate any help.
Best,
Mustafa