Other Parts Discussed in Thread: ADS1298, ADS8345
Hi!
I'm trying to communicate ADS1298 with NI-USB-8451 interface in order to get data using LabView. I'm beginning with a simple program just trying to read one register. I connect Ni-USB-8451 directly to the SPI interface of ADS1298. So, I tie RESET and PWRDOWN to high level, I use internal clock putting CLKSEL pin high and I set up the interface according to the datasheet (CPOL=0 and CPHA=1) using 4MHZ clock rate for SCLK. Also I tied both grounds, PCB & NI-USB-8451.
As I managed to make the interface run successfully with ADS8345 (I know this one is not so complicated to run), it makes me think that I've designed the program with Labview properly. Through the oscilloscope I can observe SCLK, CS and the commands which I send running well. The problem comes when I wanna read DOUT pin as I don't receive anything. Well, just '0' level. It seems like I can not communicate both devices each other.
I'd be grateful if somebody had the same problem and knows how to solve it.
Cheers!