Part Number: ADS7263
Dear TI team,
I would like to ask following questions about AVDD and DVDD in ADS7263.
1. The ADS7263 requires two power supplies, AVDD and DVDD. When VDD and DVDD do not rise at the same time at power-on, which one needs to rise first?
(Or do you need to start AVDD and DVDD at the same time?)
2. If the power is turned on in the opposite order to the one asked in step 1, does it affect the operation?
(If you answered that you need to start AVDD and DVDD at the same time in question 1, what kind of effect will the operation have if they do not start at the same time?)
Best Reagards,
Y.Ottey