Part Number: DAC53608
Hi,
With typically 0.6V and 0.8V as feedback for the power circuits, what will be the recommendation of reference, supply voltages to source[margin up to -10%] or sink[margin up to +10%]?
Thanks a lot
Rudra Prakash
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: DAC53608
Hi,
With typically 0.6V and 0.8V as feedback for the power circuits, what will be the recommendation of reference, supply voltages to source[margin up to -10%] or sink[margin up to +10%]?
Thanks a lot
Rudra Prakash
Hi,
I didn't understand your question. Can you please explain ? Are you looking for reference and power supply margin recommendations?
Regards,
AK
Yes, right. Also, want to know how do reference voltage and output voltage affect resolution?
Thank you
Rudra
Hi,
What is the variation in output voltage you are looking for? For max voltage of 0.8V from DAC, I suggest go with 1.8V reference with VDD = 3.3V
resolution is fixed 1-0 bit for DAC53608, if you are using 1.8V reference, one code change corresponds to 1.76mV. If you need more finer adjustments, you need to choose 12bit DAC. Note that 1.8V is the minimum reference input voltage for DACx3608.
Hope this clarifies.
Regards,
AK
Hi,
Thank you so much for your kind help.
Variation in output voltage is 0.6V to 0.8V.
Thanks & Regards
Rudra Prakash