This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC80501: register DEVID

Genius 9880 points

Part Number: DAC80501

Hi Team,

We have received that the register DEVID at bit 11-8 is not the same with  the register description. Thank you for your immediate response.

Below is the inquiry
"I'm getting in troubles in accessing internal register of DAC80501Z, a 16-bit Digital to Analog Converter.
I read 0x0115 as the content of the register DEVID.
From the datasheet it is somewhat contradictory what this value should be (see attachment).
Could you please clarify this ?"

  • Maynard,

    There appears to be a discrepancy in the datasheet itself as the first bit-field for the register vs the table below it. Please see below. The table contents would align with their read-back. Let me check into this and get back to you.

  • Hi,

    I've solved the problem I had in the software driver.
    I can now read the correct value from register which is 0x0115, as expected.
    Glad to know you are also fixing the datasheet.

    This ticket can be considered closed.

    Best Regards,
    Gabriele