Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLA2518: Example C codes

Part Number: TLA2518
Other Parts Discussed in Thread: TLA2528, ADS7038

Hi,

Is there any example C codes for the configuration of TLA2518?

  • Hello,

    Unfortunately there is no example code

    But the GUI for the BP-ADS7128 has a feature to export the register content and address.

    When you are using the booster pack, you can configure the device, and then export the register content for that configuration.

    There is also an EVM coming soon for the ADS7038, which is the SPI version, that can more directly be used for the TLA2528

    Regards

    Cynthia