Part Number: DAC60501
Other Parts Discussed in Thread: DAC60502, DAC70502, DAC80502
Hi,
I am just writing the software driver to support the DACx0501 and DACx0502 in our project. I found some misunderstandings in the data sheets of these DACAs.
I wonder about the device IDs of the DACx0501 and DACx0502 DACs.
The data sheet of the DACx0501 family on page 31 shows the following:
What are the right device ID for the DACs?
DAC60501Z = 2415h or 2215h, DAC70501Z = 1415h or 1215h, DAC80501Z = 0415h or 0215h ?
DAC60501M = 2495h or 2295h, DAC70501M = 1495h or 1295h, DAC80501M = 04915h or 0295h
The data sheet of the DACx0502 family shows on page 29 the following:
My question is again, what are the right device IDs for the DACs?
DAC60502 = 2215h or 2214h, DAC70502 = 1215h or 1214h, DAC80501Z = 0215h or 0214h ?
Many thanks in advance for a shortterm answer.
Kind regards
Ulrich