Part Number: ADS7956
Hi,
I am sorry that my reply was delayed in the previous post.
I share the customer situation.
>The Auto mode 1 will sampled channels that have been pre-programmed. If no channels were selected then this mode will not function properly.
>Can you provide more information about the issue? does the device previously work in mode 1, displaying the correctly pre programmed channels
>Then, without anything changing, it stops to scan and only shows channel 0?
The phenomenon occurs while the DC motor is operating. Therefore, the setting is not changed before and after the phenomenon.
>Is the customer changing from different modes and mode 1 does not work when called on?
Switching to another mode is difficult because it involves software changes by the customer.
However, it will be restored by sending the Auto Mode 1 command again.
>Does the customer have noise on the digital communications that could disrupt expected communications?
Due to the configuration of the equipment, the measurement is performed with the jumper wire pulled out, so it is an environment where it is easy to receive external noise.
Based on these, let me ask a new question.
What are the conditions under which the settings are reset (returned at power-on)?
Is there anything else that causes the ADC settings to revert to their initial state other than restarting the power supply?
Best regards,
Yuto Sakai