The proper answer to this question is to hold the RESET/PWDN pin low (as per the manual).... But I didn't anticipate wanting to put this device to sleep, so I put a pullup on the board there (i.e. always on). I'm trying to avoid running a new board and finding a free GPIO to do it the "right way".
Is there a way to put the ADS1262 into a low power sleep mode through software only? I'm also having trouble finding a spec for what the ADS1262 is supposed to draw immediately after a reset. Just upwards of 10mA... and then 25uA with the RESET/PWDN low.
Any thoughts would be greatly appreciated.