This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC088S085: Compare to AD7228A

Part Number: DAC088S085
Other Parts Discussed in Thread: TLC7226, DAC7728

Dear Team,

Here is Kevin from Delta Taiwan.

Customer is evaluating AD7228A, which I use cross reference suggest DAC088S085.

Customer will have 5 bits digital high/low signal to the device.

The device will help to transfer 5 bits high/low signal to analog voltage to MCU.

I can see AD7228A have 8 bits input pins to deal with the input 5 bits high/low signal.

But I can't see DAC088S085 have 8 input pin to deal with it.

So I don't think DAC088S085 is suitable, please suggest a more suitable device here.

BR

Kevin