This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J69: Connect two ADC on the same SPI port?

Part Number: ADS54J69


Hello Guys,

Good day.

Our just like to confirm if its okay to connect multiple ADCs on the same SPI port for this device?

Also, they want to know if the SDOUT pin is n a HiZ state when the enable signal is high?

Thanks for the confirmation!

Art

  • Art,

    You can drive multiple parts if you meet the current drive requirement of the devices in the chain.

    SDOUT is always active. It never gets tri-stated.

    Regards,

    Jim

  • Thank you very much Jim!

    Our customer has clarification though. According to him if it never gets tri-stated, how can the high level been reached on SDOUT? If both output deliver the same current, the max level would be half the voltage level of DVDD. So in his mind, a write to the ADC works but never a reading.

    Below are his connections. The input signal SEN are routet seperatly to select ADC1 or ADC2.
    The input signals SCLK and SDIN are connectet together,  also the output signal SDOUT. 

    I might direct the customer on this ticket so that he could explain better his use case.

    Thanks!

    Art

  • Art,

    You cannot short the two SDOUT's.  The SDOUT is driven even when SEN is high. This is why a write works and a read does not.

    Regards,

    Jim