This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1258: Parasitic Capacitances

Part Number: ADS1258
Other Parts Discussed in Thread: LSF0108, ADS1158,

Hi, I'm jose

I plan to use the ADS1258 in a circuit. Basically I'd like to ask about what are the parasitic capacitances associated for each pin of this Integrated Circuit, but  more precisely, I need the parasitic capacitances of the pins described below (Fig.1), because I need to use a Voltage Level Translator  (LSF0108)  for those pins, and the speed of this LSF0108 is influenced with these parasitic capacitances throught an R*C relationship where I need to get a proper value for the resistor (R)

Fig.1. pins description

Thank you for the help