This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS54J69: ADS54J69IRMP Device SPI REG value generation GUI is Required

Part Number: ADS54J69

Dear Sir 

ADS54J69IRMP Device SPI Register map value generation  GUI is Required sir 

kindly provide link to download the same sir 

thank you

regards 

Balakrishna J 

  • GUI.pptxBalakrishna,

    The GUI can be downloaded from the ADS54J69EVM product folder on the TI website. See attached.

    Regards,

    Jim

  • Dear Sir,

    Thank you very much  

    Can you please help with FPGA Interface for the same 

    1) Linux SPI Driver  or bare metal SPI Driver to interface with Xilinx MPSOC

    2) confused with register sets generated from GUI, datasheets says some set of registers and GUI Generates some sets 

    so little confusion 

    i would like to operate ADC at 320MHz clock for sampling and 2 lane per channel , both channel needs to be active and 

    LMFS   => F= 1 and K=1 

    please help out 

    thank you

    regards 

    Balakrishna J 

  • Balakrishna,

    For #1, I cannot help with this.

    For #2, per the JESD204B standard, the following equations must be meet: 17 < F * K < 1024 and 1 < K < 32

    Since you will be using LMF = 422, F = 2. To meet the equations above, we normally set K = 16.

    This part can operate in either low pass or high pass mode. I am sending  configuration file for you to try that will be configured for low pass mode with K = 16.

    With a sample rate of 320MHz, the ADC output rate will be 160MHz. SYSREF = ADC data rate / (n * K), with n = whole integer.

    The maximum SYSREF frequency you can use is 160M / 16 = 10MHz.

    Give this a try.

    Regards,

    Jim

     

    0x0000 0x81
    0x0011 0x80
    0x0056 0x08
    0x0039 0xC0
    0x003A 0x40
    0x0059 0x20
    0x4004 0x68
    0x4003 0x00
    0x4002 0x00
    0x4001 0x00
    0x60F7 0x01
    0x6041 0x12 
    0x604D 0x08 
    0x6052 0x80 
    0x6072 0x08 
    0x6000 0x01 
    0x6000 0x00 
    0x4004 0x69
    0x4003 0x00
    0x6000 0x80
    0x6006 0x0F
    0x6001 0x31
    0x6031 0x0A 
    0x6032 0x0A
    0x4004 0x6A
    0x4003 0x00
    0x6012 0x02 
    0x6016 0x00
    0x4004 0x61
    0x4003 0x00
    0x6068 0x02