Part Number: ADS1148
Other Parts Discussed in Thread: ADS1243, ADS1241, ADS1242, ADS1248, ADS1240,
Dear All,
I am planning to use ADS1148IPW for Pirani vacuum gauge sensor.
Schematic is as below:
However, looking at the calculations, it requires REF voltage of 200 mV.
Is it possible to use 200 mV directly as suggested or this will affect the resolution? If I use 2.047 V for example, and use the gain, how to divide it so no temp drift, etc. present errors. The filament of the Pirani sensor is also about 4 Ohms, and the current through it is 0,4 A.. Any help as suggestions and opinions is more appreciated.
Best Regards,
Stanislav