This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7718: gain setting

Part Number: DAC7718


Hi,

I have similar question to below link.

https://e2e.ti.com/support/archive/internal/int-precision_data_converters/f/75/t/294750?tisearch=e2e-sitesearch&keymatch=dac7718%20gain

0.0015% is right value in 16bits setting.

At 12 bits setting, it has to be 0.024% FSR/step

Could you explain about it?

Thanks.

  • David,

    You are correct - the value for the 12-bit part should be 0.024% FSR. Our Systems team was informed of this typo from the 16-bit part and was to correct it, but it doesn't look like that has happened. I will try to get this fixed again.