Part Number: DAC7760
Hello,
I have a question for DAC7760 specification.
The datasheet says that DIN pin and SCLK pin are Schmitt-trigger inputs.
Usually parameters like V_T+/V_T-/Hysteresis(V_T+ - V_T-) are specified for Schmitt-trigger inputs.
But this datasheet just defines V_IH and V_IL.
I think this V_IH/IL are not for these Schmitt-trigger type but for normal inputs
Could you tell me V_T+ and V_T- for these Schmitt-trigger inputs.
And there is “Hysteresis voltage” parameter in the datasheet in P9. Is it for these Schmitt-trigger inputs?
Regards,
Oba