Part Number: ADS8638
Looking for Python source code for ADS28638 to control and set up device or any other related ADC part.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS8638
Looking for Python source code for ADS28638 to control and set up device or any other related ADC part.
Hi Wesley,
Unfortunately, there is no example code for this ADC. Is this a new design? If so, ADS8668 ADC family can be a good solution for you, which has a lot of features you can benefit from, for instance, an integrated Analog Front-End (AFE) including PGA, LPF filter and ADC driver on each channel, single +5V power supply but can support +/-10V direct bipolar input signals.
Thanks&Regards,
Dale