Other Parts Discussed in Thread: , DAC11001A, DAC8832
Hi,
I need to generate 2 voltage signals of 500 KHz frequency and +/-5V output range with an accuracy of 16 bits. By going through the products DAC8814 seems good. However unlike ADC where the throughput is clearly mentioned, DAC output rate is given as settling time.
1) DAC8814 is having a settling time of 0.5us. I believe this for 0000h to FFFFh transition. Since I am generating a sinusoidal signal, whether this will create an issue.
2) Is there any other DAC with better than DAC8814 satisfying my requirements.
3) I am planning to interface it with F280049C Launchpad kit. Hope it wont create any issue.
4) The DAC is current output and I need voltage output. Whether I can use the DAC8814EVM for initial prototyping of this application.
Thanks and Regards
Karthik R