Part Number: ADS1235EVM
Other Parts Discussed in Thread: ADS1235
Hi,
I had some questions about the ADS1235
1. In the output to the data analysis window there are output values for
ADC0 and CRC0. What is CRC0?
2. When I use the collect data button in the Data Analysis screen, or when I submit a Collect n command from the script window
It always resets to delete all the previously received data. I would like to collect 19 sets of 20 data points to be able to change the input signal to cover the entire range of the input scale.
Is there a way to write a script that will add data to the output but not clear the existing set?
3. I read through the calibration instructions but not sure I am following the part about using 95% for full scale by setting FSCAL[2.0]=3CCCCCh.
When you do that do you use a full scale input signal or so you need to use a 95% full scale input signal?
What are the commands to set the offset and the full scale, are they SYOCAL and SYGCAL? What is the SFOCAL self offset calibration used for?
Thanks for the help,
Adam