Part Number: WAVEVISION5
hello,
Will Wavevision5 allow the time-domain digital input samples (output samples from ADC) and/or the FFT spectra dats to be exported to a txt/csv file etc ...
Kind Regards,
Rajan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: WAVEVISION5
hello,
Will Wavevision5 allow the time-domain digital input samples (output samples from ADC) and/or the FFT spectra dats to be exported to a txt/csv file etc ...
Kind Regards,
Rajan
Hi Rajan,
Wavevision5 does not allow you to directly save the plot as a txt/csv file. However, there may be a way to save the channel data. What you can try is import a csv file that contains data and then you can acquire your data on that same channel, overwriting what you imported. Then when you save your channel data to a file it should save as a csv file.
Regards,
David Chaparro
David,
thank you for your reply.
what not just save the channel data? how is this done?
thank you
rajan
Rajan,
To save the channel data to a txt/csv file what you have to do is go to the Channels Tab on the left side of the Wavevision5 application. You can click the save channel data to file. Then in the Channel Data file Name box you can change the file extension to txt or csv. This will save the application to that type, there is no need to import a different csv file as I had mentioned before.
Regards,
David Chaparro
I don't see the following:
click the save channel data to file
will this operation save the input time domain data or the output frequency spectrum
thank you