Part Number: DAC38J84
Hi
I have tried NCO Reset through SYSREF .
I have generated 100 MHz NCO Signal and doing the Reset on Sysref Pulse.
I have observed that there is 180 degrees phase change on doing the NCO Reset.
Why particularly there is 180 degrees phase change. Any Specific Reason ??
Ideally after reset, it must start with 0 degrees phase, but why I am getting 180 degrees ?? I have attached the Picture
In my final application I need to use NCO of 600 MHz . So it is difficult to observe it on Oscilloscope.
So How to make sure that NCO reset is done at 600MHz (Mixed with Singletone and LFM Data) ???