Part Number: DDC11XEVM-PDK
Hello. I recently acquired the DDC11XEVM-PDK. I've got everything working well with the evaluation software but would like to integrate the evaluation module into my application through Labview. I found on the forums the Labview VIs_to_DLL.zip as well as the DLL code folder DDC11xEVM_DLL_Files.zip. The Labview vis were incomplete and contained only the XferINTDatIn and XferINTDataOut. The FPGA registers can't be configured nor the data captured. I tried to use the labview DLL import wizard with the USB_IO_for_VB6.dll and the corresponding header file. I then built up the VIs according to the USB_IO_for_VB6_DLL_User_guide. I'm having difficulty writing to the FPGA using the WriteFPGARegsC function which just causes Labview to crash due to access violation. My first question is whether there are updated VIs or other files compiled together since I'm having to pull from so many sources and whether I may be conflating operation between the DDC246EVM and the DDC11XEVM-PDK. I appreciate any advice others may have to get this operational.
Thanks,
-Phillip