Other Parts Discussed in Thread: ADS1119,
Hi Team,
I am using ADS112C04 for temperature measurement. Normally I use thermocouple with this IC. But my question is can I replace the thermocouple with an NTC thermistor in the same thermocouple circuit? . Also my reference for the IC in therrmocouple measurement is at 1V will it affect my thermistor measurement reading, if it is possible to use a thermistor. Since I came across something like 'the reference should be same for thermistor measurement and ADC'. If thermistor reading is possible can I use the equation in ADS1119's datasheet to get temperature or resistance value back.
Thank you,
Vineeth N