Other Parts Discussed in Thread: ADCPRO
I see a symptom similar to that in the "Related Thread" above, but over there the discussion diverted and I see no resolution to the original question.
I am using ADCPro 2.0.1 with ADS1278EVM plugin 2.0.0 [MMB0] (downloaded last week) on a 32-bit Windows 7 system. (I had similar symptoms on a 64-bit Win10 machine, but after seeing that Win10 is unsupported I moved.)
I cannot get ADCPro to collect data reliably. Out of maybe 40 attempts over this week, I have only twice succeeded in running a session for more than about 2 minutes. The symptom is a LabView error (see below) either during setup or during data collection, after which the program (per Windows) "stops working". The messages seem to point to the USB driver, but I leave that to the experts.
What I am asking it to do is (seemingly) modest: Single channel, Low Power or High Resolution mode (52ksps), Scope or FFT application, no peculiar settings.
I don't know how to diagnose this further. Can someone suggest something? Thanks.
-------------
Each of these errors is from a different run (since the program crashed afterward). Maybe the tracebacks mean something to someone.
The first error is right after loading the plug-in, selecting the Settings tab.
The second is trying to select a new Operating Mode in the Settings tab.
The third occurred after running the scope for < 1 minute.